{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does the 8538 combination starters come with external reset button?

Issue:
For an enclosed combination starter 8538 other than NEMA 12, does it come with external reset as standard or need to order it separately?

Product Line:
Class 8538 and 8539T ype S combination starters

Environment:
Applies to all SquareD enclosed combination starters

Cause:
There is a need to know if external reset button should be bought separately or is included as standard

Resolution:
All SquareD enclosed starters come with external reset as standard, unless otherwise stated in the digest/catalog footnotes

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: