Issue
A user may want to add a custom image/logo in place of the default "Schneider Electric" logo that is displayed on reports.

Product Line
ION Enterprise 6.0
SPM 7.0.1
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Web Applications "Reports"
Cause
It may be desired to replace the default image/logo displayed on reports
Resolution
For ION Enterprise 6.0 and SPM 7.0.1:
For PME 8.0 and PME 7.2.x:
For PME 8.1:
For PME 8.2:
b. Click Finish to add it to the image repository.
A user may want to add a custom image/logo in place of the default "Schneider Electric" logo that is displayed on reports.
Product Line
ION Enterprise 6.0
SPM 7.0.1
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
Web Applications "Reports"
Cause
It may be desired to replace the default image/logo displayed on reports
Resolution
For ION Enterprise 6.0 and SPM 7.0.1:
- Navigate to http://localhost/Reports$ION or http://localhost/Reports or http://localhost/ReportsION or http://localhost/Reports_ION (this is dependent on how the system is set up)
- Next, navigate through ION Reports --> ION Reports Packs --> Default Reports
- Click on Report-Logo.jpg. This file needs to be replaced with a custom logo file with the same name (review screenshot below)
- Note: The image file is required to be no larger than 250x100
- Click on Upload File'
- Browse to the custom logo file and make sure the name is Report-Logo.jpg
- Now, every report that is run from the Default Report Pack will have the new custom logo at the top of the report.
For PME 8.0 and PME 7.2.x:
- Navigate to the following directory:
...\Schneider Electric\Power Monitoring Expert\web\ReportDepot\ION Reports\ION Report Packs\Default Reports
- There will be a JPEG file in the folder named Report-Logo. The image file is required to be no larger than 250x100
- If you replace the image with a different image that is named Report-Logo, the new image will be displayed on reports (as shown in the screenshot below)
For PME 8.1:
- Navigate to the following directory:
...\Schneider Electric\Power Monitoring Expert\config\reports
- There will be a JPEG file in the folder named Report-Logo. The image file is required to be no larger than 250x100
- If you replace the image with a different image that is named Report-Logo, the new image will be displayed on reports (as shown in the screenshot below)
For PME 8.2:
- Navigate to the following directory:
...\Schneider Electric\Power Monitoring Expert\web\App_Data\images\logo
- There will be a JPEG file in the folder named Report-Logo. The image file is required to be no larger than 250x100
- If you replace the image with a different image that is named Report-Logo the new image will be displayed on reports (as shown in the screenshot below)
- Open Web Applications
- In SETTINGS, open the Settings Library > Personalization > Report Theme.
- Under Report Logo, click Select to open the Select Report Logo Image dialog.
- Select an image currently available in the repository, or:
b. Click Finish to add it to the image repository.
- Click OK to complete your selection.
- Click Save to apply the changed settings.
- If you replace the image with a different image the new image will be displayed on reports (as shown in the screenshot below)
Released for:Schneider Electric Canada