Search FAQs
Do merchandised, RTI NF and NQ Panelboards include a neutral as standard?
Issue:
Neutral on all merchandised, RTI NF and NQ panelboards
Product Line:
NF, NQ Panelboards.
Environment:
Merchandised NF and NQ panelboards sold and supported in the USA.
Cause:
Does the RTI panelboards include a neutral assembly as standard?
Resolution:
Yes, the NF and NQ panels include a standard neutral that is sized for the circuit count and amperage of the individual panel.
Below are field installed options.
Notes
Neutral on all merchandised, RTI NF and NQ panelboards
Product Line:
NF, NQ Panelboards.
Environment:
Merchandised NF and NQ panelboards sold and supported in the USA.
Cause:
Does the RTI panelboards include a neutral assembly as standard?
Resolution:
Yes, the NF and NQ panels include a standard neutral that is sized for the circuit count and amperage of the individual panel.
Below are field installed options.
NQ Merchandised Neutrals | ||
Amp (A) | 200% Neutral kit | 100% CU Neutral Kit |
100 | NQNL1 | NQN1CU |
225 | NQNL2 or NQNL2ACCY | NQN2CU |
400 | NQNL4 | NQN6CU |
600 | Not Available | NQN6CU |
Notes
- The NQNL4 is not to be used with SFL, FTL, or SFB. These combinations are factory assembled only.
- For 225A panel with SFL, FTL, or SFB, use NQNL2ACCY (enclosure size increases by 6 inches). Otherwise, use NQNL2.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: