{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is included in the value pack HOM3060M200PCAFVP?
Issue:
Determining value pack components

Product Line:
Homeline load centers

Resolution:
It includes;
(1) HOM3060M200PC (Homeline plug-on neutral, 200Amp, 30space- 60 circuit maximum, indoor, main breaker load center),
(3) HOM115PCAFI (HOM, Plug-on Neutral, 15 A, single-pole Combination Arc Fault branch circuit breaker.
(3) HOM120 (Homeline 20 A single-pole branch circuit breaker)
(2) HOM230 (Homeline 30 A, double-pole branch circuit breaker)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: