{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the STRV00121 front display module, FDM121, for PowerPacT H, J, and L frame circuit breakers be used with multiple breakers?

Issue:
Can I connect multiple breakers to the FDM121?

Product Line:
Molded Case Circuit Breakers

Resolution:
No. The STRV00121 front display module, FDM121, can only be use with one breaker. For multiple breakers, an FDM128 is required.

Schneider Electric Canada

Attachment(s)

FDM.jpgFDM.jpg [8.82 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: