{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NQOB panelboards and branch circuit breakers
Issue:
What branch breakers does the obsolete NQOB panelboard accept?  Is there any mounting hardware required for them?

Product Line:
Obsolete NQOB Panelboards

Resolution:
NQOB panelboards accept QOB branch breakers, and a 60 A maximum branch circuit breaker can be installed into NQOB column width panelboard.  No mounting hardware is required for these.


Note: The QOB-VH and QHB breakers did not exist during the life of the NQOB interior and as a result were never UL/CSA tested or approved for use in the panel. They are not designed to be installed in the NQOB interior.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.