Search FAQs
Are a neutral and neutral CT available for use with a PowerPacT L frame 400 - 600 A breaker installed in an L600AWK enclosure?
Issue:
Product Design Features
Product Line:
Circuit Breaker Enclosure
Resolution:
The L600AWK enclosure is suitable to accept the SN400LA, SNC400LX, SNC800LX, or the SN1000MA solid neutral assemblies.
When mounting the L Frame PowerPacT breaker with the LSIG function, the solid neutral with current transformer is required, so use the SN600LXCT (purchase neutral CT separately, part number S432575).
Product Design Features
Product Line:
Circuit Breaker Enclosure
Resolution:
The L600AWK enclosure is suitable to accept the SN400LA, SNC400LX, SNC800LX, or the SN1000MA solid neutral assemblies.
When mounting the L Frame PowerPacT breaker with the LSIG function, the solid neutral with current transformer is required, so use the SN600LXCT (purchase neutral CT separately, part number S432575).
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: