{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the tripping current for a Multi 9 GFP?
Issue:
What is the tripping current for a Multi 9 GFP Ground Fault Protector?

Product Line:
Circuit breakers

Resolution:
Tripping currents are as follows:
GFP30     Must trip beyond 29.9 mA; must not trip below 22.1 mA
GFP100     Must trip beyond 98.9 mA; must not trip below 73.1 mA
GFP300     Must trip beyond 299 mA; must not trip below 221 mA

Schneider Electric Canada