Issue:
Will the EDPA fixed padlock attachment physically fit onto the EDB-EPD Ground Fault Circuit Breakers?
Product Line:
Circuit Breakers
Resolution:
The EDPA cannot be installed onto an EPD ground fault circuit breaker.
The EDPA must be attached to the breaker using slots in each end of the breaker escutcheon. Standard EDB, EGB, and EJB circuit breakers without EPD suffix (series 2 and higher), have these slots (see picture A below). EPD ground fault circuit breakers do not have these slots (see picture B below), so the EDPA cannot be attached.
Picture A
Standard EDB Circuit Breakers without EPD suffix, series 2 and higher (slots)
EDPA can be used.
Picture B
EDB-EPD Ground Fault Circuit Breakers (no slots)
EDPA cannot be used.