{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the maximum loads of EDB, EGB, EJB accessories?
Issue:
Maximum load of e-frame breaker accessories

Product Line:
E-frame Breakers/NF Panels

Resolution:
Auxiliary Switch: Maximum load of 10 A at 120 Vac, 50/60 Hz
Alarm Switch: Maximum load of 7 A at 120 Vac, 50/60 Hz
Shunt Trip: Coil burden of 288 VA

Schneider Electric Canada