{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does Schneider offer a feed-thru tap off for feeder busway on a vertical riser run?

Issue:
Feed through tap box for busway

Product
Line:Busway

Environment:
I-Line II

Cause:
Product Offering

Resolution:
We can build an in-line Reduced Capacity Tap Box. This is 24" h with 10" stubs on either end.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: