Search FAQs
Which PM5000 series meters are available in the US and Canada? What software supports the PM5000 series meters?
Issue
Which PM5000 series meters are available in the US and Canada? What software supports the PM5000 series meters?
Product Line
PowerLogic PM5000 Series Meters
Environment
Energy Monitoring Systems with PM5000 series meters.
Cause
To determine PM5000 Series Meter compatibility and sales options.
Resolution
Schneider Electric manufactures multiple different models of the PM5000 series globally which are designed for different market needs. In the USA and Canada, the following models are available:
METSEPM5110, METSEPM5350, METSEPM5340, METSEPM5560, METSEPM5563
NOTE: The PM5350 is NOT available in the USA or Canada.
![PM5000 meter types PM5000 meter types](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zpoJQAQ&oid=00DA0000000abSm)
The PM5000 series meters are natively supported in StruxureWare Power Monitoring Expert (PME) 7.2.2 and greater.
The PM5000 series meters can be added to a StruxureWare Power Monitoring Expert 7.2.0, 7.2.1, and 7.0.1 via an optional Installer. Device driver installs are available on Schneider-Electric.com in the Downloads Center.
Which PM5000 series meters are available in the US and Canada? What software supports the PM5000 series meters?
Product Line
PowerLogic PM5000 Series Meters
Environment
Energy Monitoring Systems with PM5000 series meters.
Cause
To determine PM5000 Series Meter compatibility and sales options.
Resolution
Schneider Electric manufactures multiple different models of the PM5000 series globally which are designed for different market needs. In the USA and Canada, the following models are available:
METSEPM5110, METSEPM5350, METSEPM5340, METSEPM5560, METSEPM5563
NOTE: The PM5350 is NOT available in the USA or Canada.
The PM5000 series meters are natively supported in StruxureWare Power Monitoring Expert (PME) 7.2.2 and greater.
The PM5000 series meters can be added to a StruxureWare Power Monitoring Expert 7.2.0, 7.2.1, and 7.0.1 via an optional Installer. Device driver installs are available on Schneider-Electric.com in the Downloads Center.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: