Search FAQs
What parts are needed to make up a reversing Tesys U line motor starter?
Issue:
Parts to make up a reversing TeSys U line motor starter
Product Line:
Contactors and Starters-IEC
Environment:
TeSys U Open Motor Starter
Cause:
Building a reversing TeSys U line motor starter
Resolution:
There are multiple ways to make a u line reversing starter. The LU2B*2 can be ordered with a control module to make up a starter. You can also order the LUB*20 with the LU2MB0 reversing module, the LU9M1 coil terminal, and the LU9MR1C control block
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: