{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Tesys T with Modbus over Ethernet communicate with Rockwell RSLogix 5000?

Issue:
Can the Tesys T with Modbus over Ethernet communicate with Rockwell RSLogix 5000?

Product Line:
All Schneider Electric products

Environment:
Products sold and used in the United States

Cause:
Customer is using a Rockwell PLC with our Tesys T overload relay


Resolution:
The TeSys T Ethernet device can communicate if the Rockwell unit is communicating via Modbus TCP over Ethernet or EtherNet IP, if the device communicates using devicenet, a devicenet Tesys T will need to be used.

The following quick start guides can be used to set up the Ethernet or Devicenet TeSys Ts:
https://www.se.com/ww/en/download/document/DOCA0119EN/

https://www.se.com/ww/en/download/document/1639575_02A55/

Schneider Electric Canada