{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of the M580 SD card?
The SD memory card on the M580 is used to backup the application in the event of a hardware issue.
The application and any saved data (%MW initial values) on the SD card cannot be accessed via USB or FTP.

The memory card with application and backed up initial value data can be inserted in a new CPU to load and run the application.

****State Ram is not kept on the SD card when initializing an M580****

Schneider Electric Canada