{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the flexible cable mechanism for the FAL circuit breaker like the FAL36100?
Issue:
What is the flexible cable mechanism for the FAL circuit breaker like the FAL36100?

Product Line:
Class 9422 Flexible Cable Mechanisms

Cause:
Need a cable operating mechanism for a circuit in a custom enclosure or panel.

Resolution:
Below are the available part numbers.
Circuit Breaker TypeNumber of PolesCable MechanismCable Mechanisms with A1 Handle For Types 1, 3, 3R, 12
Total LengthFlexible LengthTypeType
FAL, FHL336"22"9422CFA309422CFA31
60"46"9422CFA509422CFA51
120"106"9422CFA109422CFA11

See instruction bulletin, 50006-370-01

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: