{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are auxiliary contact available for 8903 Type L 2 pole contactor?

Issue:
What is the part number for an auxiliary contact for a 2 pole 8903 lighting contactor?

Product Line:
8903LO20, 8903LA20, 8903LW20, 8903LWW20, 8903LH20, 8903LF20, 8903LG20
8903LXO20, 8903LXA20, 8903LXW20, 8903LXWW20, 8903LXF20, 8903LXG20

Environment:
US product

Cause:
There is no part listed for an auxiliary contact

Resolution:
There is no auxiliary contact available for this device.  Additional power poles can be used to function as auxiliary contacts.  On a two pole device, fill in the missing poles with a power contact from kit  9998RA5B, one spring seat 31071-019-01, and one contact support 31071-018-01.  This will give one additional contact which can be converted from NO to NC and vice versa.

Schneider Electric Canada