{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the 9999SA2 and 9999SA10 have the same functionality?

Issue:
What's the difference between the field kit 9999SA2 for start/stop and 9999SA10 for on/off?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9999 NEMA contactor/starter acessories

Resolution:
The two units only differ in the legend plate which comes with them.  Functionally they are identical.

Schneider Electric Canada