{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the voltage code for a D40 suffix for a 9070T100D40 ?
Issue:
What are the voltage ratings for the D40 voltage code for a 9070 type transformer?

Product Line:
control transformer, CPT

Environment:
9070T

Resolution:
The voltage code D40 indicates single phase, 208/240/380/416/480V on the primary and 120V on the secondary.

Schneider Electric Canada