Search FAQs
What is the maximum amperage that can be fed into the SR69064A solar ready kit used with certain CSED panels?
Issue:
Application
Product Line:
CSED
Resolution:
The installing electrical contractor should consult the latest National Electrical Code (NFPA 70) that is being enforced in the installation area.
The SR69064A solar ready kit includes (2) phase lugs, (1) neutral lug, (1) interactive inverter label, and installation instructions. The lugs provided in the SR69064A provides for a maximum of (1) #6 - 2/0 AWG Al or (1) #10 - 2/0 Cu conductors. Based on the 75 degree C conductor ampacity, #2/0 Al is rated 135 ampere and #2/0 Cu is rated 175 ampere.
NOTE: The lugs in the kit are ONLY UL tested and Listed for 75 degree wire and if 90 degree wire is used, the installer Must follow the 75 degree table in the NEC.
Application
Product Line:
CSED
Resolution:
The installing electrical contractor should consult the latest National Electrical Code (NFPA 70) that is being enforced in the installation area.
The SR69064A solar ready kit includes (2) phase lugs, (1) neutral lug, (1) interactive inverter label, and installation instructions. The lugs provided in the SR69064A provides for a maximum of (1) #6 - 2/0 AWG Al or (1) #10 - 2/0 Cu conductors. Based on the 75 degree C conductor ampacity, #2/0 Al is rated 135 ampere and #2/0 Cu is rated 175 ampere.
NOTE: The lugs in the kit are ONLY UL tested and Listed for 75 degree wire and if 90 degree wire is used, the installer Must follow the 75 degree table in the NEC.
Released for:Schneider Electric Canada
Explore more
Category:
Explore more
Category: