{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can 50 degree C rated PowerPacT breakers (-CA suffix) go into I-line panels?

Issue:
Using 50 degree C breakers in I-Line panelboards

Product Line:
Molded Case Circuit Breakers and Panelboards

Resolution:
Yes, the circuit breakers that are factory calibrated for a 50°C ambient temperature with -CA suffix may be used in I line panelboards.

NOTE:
Circuit breakers with special thermal calibration such as -CA suffix are not UL Listed.
The CA suffix is only available for PowerPacT H, J, and Q frame thermal magnetic circuit breakers.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: