{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are Homeline, NEMA 1 load center covers available without an integral door?
Issue:
Product Features

Product Line:
Load Center

Resolution:
The only Homeline, NEMA 1 load center covers that are not provided with an integral door that provide access to the circuit breakers would include the covers that are provided with the following load centers:

HOM24L70F
HOM24L70S
HOM48L125GC
HOM612L100F
HOM612L100S
HOM60120L225PC * ( There is a Door Kit available for this load center, the part number is QOCDK60)
HOM60120M200PC* (There is a Door Kit available for this load center, the part number is QOCDK60)

All other Homeline, NEMA 1 load center covers are provided with an integral door and are not available without the integral door.

Schneider Electric Canada