Issue:
What overloads can be used with an 8910DP definite purpose contactor?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
8910 Types DP, DPA Definite Purpose Contactors
Cause:
These contactors do not list an overload but can be ordered with one as an 8911DP type starter.
Resolution:
These contactors do not have a dedicated overload that can be ordered separately. The easiest solution is to order an LRD type bimetallic overload and separately mount it with an adapter.