Search FAQs
How to select Full Voltage NEMA Contactor or Starter Part Numbers?
Issue:
Product selection of a Schneider Electric NEMA Style Contactor or Starter for a new installation.
Product Line:
NEMA Contactors, Manual, Fractional Horse Power, Full Voltage, Reversing, and Combination Starters , Definite Purpose Contactors and Starters , Lighting Contactors
Environment:
Contactors and Starters Sold in the United States
Resolution:
Please refer to our Online Digest Chapter 16 which provides selection assistance for our NEMA Type S contactors and starters:
Product selection of a Schneider Electric NEMA Style Contactor or Starter for a new installation.
Product Line:
NEMA Contactors, Manual, Fractional Horse Power, Full Voltage, Reversing, and Combination Starters , Definite Purpose Contactors and Starters , Lighting Contactors
Environment:
Contactors and Starters Sold in the United States
Resolution:
Please refer to our Online Digest Chapter 16 which provides selection assistance for our NEMA Type S contactors and starters:
- From the Digest Section 16, Choose from the following:
- Manual Starters and Switches (Refer to Product Selector)
- Full Voltage and Combinations Contactors & Starter
- Definite Purpose Contactors & Starters
- Lighting Contactors
- Choose Product Subset (Except Lighting Contactors):
- Reversing
- Non-Reversing
- Two Speed
- Choose Power Source/Application:
- Single Phase
- 3 Phase
- DC (Does Schneider offer DC rated NEMA Contactors and Starters?)
- Choose Voltage , Poles and Maximum Horsepower
- Choose Enclosure Type and Accessories
- If standard Overload Relay is chosen, Select Thermal Units based on Motor FLA
- Refer to this Catalog Numbering System to validate your part number