{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is there a mushroom guard for the 9001KR16 operator?

Issue:
Is there a mushroom guard for the 9001KR16 operator?

Product Line:
30mm 9001K Push buttons

Environment:
Push Buttons and Operators

Resolution:
No, we do not offer a mushroom guard for the 9001KR16 trigger action, turn to release mushroom operator.  They may consider the guarded enclosure part number 9001KYG1, gray box and cover or the 9001KYG1Y gray box with yellow cover.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: