Issue:
Define suffix TX on an H or J-frame breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
TX suffix indicates metric terminal nuts factory installed on the ON end of the breaker. They can also be field installed with the following part numbers:
S37426 for H frame (contains two terminal nuts)
S37428 for J frame (contains two terminal nuts)
Define suffix TX on an H or J-frame breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
TX suffix indicates metric terminal nuts factory installed on the ON end of the breaker. They can also be field installed with the following part numbers:
S37426 for H frame (contains two terminal nuts)
S37428 for J frame (contains two terminal nuts)