{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to view trip history on PowerPacT H, J, and L frame Micrologic trip units?
Issue:
Is there a record of trip history that can be seen on the trip unit screen of Powerpact H, J and L breakers?

Product Line:
Molded Case Circuit Breakers

Resolution:
Trip history is stored in the trip unit, but it is not visible on the trip unit screen.
Trip history can be obtained using the following:
(1) From a front display module FDM121 (if connected to the breaker)
(2) Remotely, using communications

Schneider Electric Canada