{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How do you install a QOB3110VH, QOB3125VH, QOB3150VH breaker into a NQOD, or NQ Panelboard ?
Issue:
How do you install a QOB3110VH, QOB3125VH, QOB3150VH breaker into a NQOD, or NQ Panelboard ?

Product Line:
NQOD & NQ Panelboards

Environment:
All models

Cause:
Process clarification

Resolution:
When installing the breaker, which will occupy 6 vertical pole spaces, the bolt on buss connections must be pulled out from underneath the breaker. After exposing the connections , screw them into the phase buss fingers of the interior. A 20A adjacent breaker is the largest that can be used in a NQOD Panel, whereas a 40A adjacent branch breaker is the largest for a NQ Panel.

Schneider Electric Canada