{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is hardware provided to mount the channels for the NEMA 3R and NEMA 1 I-Line enclosures, such as catalog HC4259WP and HC4250DB?
Issue:
Mounting hardware for outdoor box channel
Product Line:
Panelboards
Environment:
I-Line , Nema 3R
Cause:
Product Selection
Resolution:
There is no hardware provided to mount the enclosure into the wall since it is unknown what kind of surface or fastener is needed. The customer always provides.

Schneider Electric Canada