{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the I-Line panel Sub-feed Lug kit for 1200a that meets NFPA 70E and CSA Z462 requirements?

Issue:
SFL Kit for 1200A I-Line panels.

Product Line:
Panelboards

Environment:
I-Line

Cause:
Special barriers

Resolution:
Use a SL1200P5  for 4- #3/0-500kcmil cables,  a SL1200P6 for 3-350-600kcmil cables or a SL1200P7 for 3-3/0-750kcmil cable, and S33931 for 4 - #3/0 - 500KCMIL. All units
take 9" of mounting space. These items can only be used in HCW, HCP, HCPSU, and HCRU I-line panels.

Schneider Electric Canada