{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a limit to the number of ZBRA1 antennae which can be used in conjunction with each other?
Issue:
What is the maximum number of ZBRA1 antennae that can be used together?

Product Line:
Push Buttons and Operator Interface

Environment:
Wireless Pushbuttons

Cause:
There is no specification with regards to this application.

Resolution:
There is no actual limit to the number of antennae which can be used in conjunction with each other.  So long as there is a viable way to power each antenna along the way, an unlimited number of antennae can be used to extend a signal.

Schneider Electric Canada