{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are NEMA 1 general purpose enclosures available for 8910DPA contactors?
Issue:
I need an enclosure for an 8910DPA contactor

Product Line:
NEMA Contactors and Starters

Environment:
8910 Definite Purpose Contactors

Cause:
Can not find it in the Digest

Resolution:
For the 8910DP, 1 and 2 pole devices, the 8910DPA 20-40A, 2 and 3 pole contactors: 9991DPG1

Schneider Electric Canada