{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the default Baud Rate and Parity of the CM 100/200 series meters
Issue
A user needs the default baud rate and parity information for the CM100/200 series meters for communication.

Product Line
CM100
CM200

Environment
Serial Communications

Cause
A meter reset has been performed restoring the meter to default settings

Resolution
The default parity on the CM 100/200 series meters is even while the default baud rate is 9600

Schneider Electric Canada