{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the padlock attachments for the QOM1 and QOM2 main breakers used in QO and Homeline load centers?
Issue:
QOM1 and QOM2 padlock attachments

Product Line:
QOM1 and QOM2 Main breakers

Resolution:
The padlock attachment for the QOM1 is part number QOM1PA.
The padlock attachment for the QOM2 is part number QOM2PA
Both padlock attachments are for locking in the OFF position only. There are no attachments available to lock in the ON position.

Schneider Electric Canada