{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the RC3040M200SL Series M01?
Issue:
Current design repair parts

Product Line:
Combination Service Entrance Devices

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE:
WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field replaceable:
Meter Cover - 7329431450 (Includes latch)
Load Center Cover - 7329421550 (Includes hinges)
Load Center Cover Mounting Screws - (4) 2159417121
Dead Front Interior Trim - 7329421401
Dead Front Interior Trim Mounting Screws - 4020513001K (This kit contains 10 screws. Only 2 screws are required to mount the interior trim)
Load Center Interior - 4056184950 (Does not include main breaker, see Main Breaker below)
Load Center Interior Mounting Screws - (8) 2153217161
Main Breaker - QOM2200VH, Mounting Hardware - (2) 2342702001 Keps Nuts
Lever Bypass Meter Socket Assembly and Mounting Pan - 7329442050 (Includes the complete lever bypass meter socket and mounting pan)
Load Side Meter Socket Bus Connectors - 7329441350 (this part number is the same for both the A and B phase and attaches to the load side of the meter socket)
Keps Nuts for Load Side Meter Socket Bus Connectors - (2) 2342702400 (attaches the bus connectors to the load side of the meter socket assembly)
Main Circuit Breaker Bus Connectors - 7329441401 (this part number is the same for both the A and B phase. These connectors attach to the above load side meter socket bus connectors and to the line side of the main breaker)
Keps Nuts for Main Circuit Breaker Bus Connectors - (2) 2342702001 (connects the load side meter socket bus connectors to the main circuit breaker bus connectors).
Load Center Cover Latch - 4056314701 (this is the latch that attaches to the side of the enclosure for the load center cover)
Rivet for load center cover latch - 2410712140 (rivet used to attach the LC Cover latch to the side of the enclosure)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.



Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: