{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the wire range for the VCEL07512H1 Versa-Crimp (TM) Compression Lug?
Issue:
Product details

Product Line:
Heavy Duty Switch Accessories

Resolution:
The lug wire range is 500 - 750 kcmil aluminum or 500 kcmil copper

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: