Issue:
Drip shield available to convert a box HC265B to be rated at NEMA 2 rather than NEMA 1
Product Line:
I line panelboards.HC3248B HC3264B HC3273B HC3291B
Environment:
Products sold in Canada
Cause:
Availability.
Resolution:
The sprinkler proof endwall is catalog number HCT2DH32. This is a Type 2 Driphood, mostly used in Canada.
Drip shield available to convert a box HC265B to be rated at NEMA 2 rather than NEMA 1
Product Line:
I line panelboards.HC3248B HC3264B HC3273B HC3291B
Environment:
Products sold in Canada
Cause:
Availability.
Resolution:
The sprinkler proof endwall is catalog number HCT2DH32. This is a Type 2 Driphood, mostly used in Canada.