{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the PQ3620G an exact replacement for the old PQ3620 plug-in units.
Issue:
Replacement for the old PQ3620 plug-in units

Product Line:
I-Line II Busway

Environment:
Fusible Plug in Units, 200 amp, 120/208 Vac (240 Vac Max) 4-Pole, 3 Fuse + G

Cause:
There is a need to know if the PQ3620G can be used in place of the PQ3620.

Resolution:
Yes, however, the ground stab may need to be removed if used on some of the older I-line busway products that had no opening allowing for newer integral ground connection

Schneider Electric Canada