{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
GVA01 compatibility with GV3P
Issue:
Which starters can the GVA01 contact block be used with?

Product Line:
GV Manual Motor Starters

Environment:
US Product

Cause:
Customers crossing their older starters forward need to know compatibility with contact blocks as well.

Resolution:
The GVA01 contact block was only for use with GV3M manual motor starters.  If a Customer is switching to a GV3P type starter, then new auxiliary contacts must be purchased.

Schneider Electric Canada