Search FAQs
PM5000 Default IP Address and the Login User Name and Password
Issue
Default IP address and login information unknown to login to the webpage and FTP server of PM5000 series meter
Product Line
PM5000 Series
Environment
Web server
Resolution
The default IP address is 169.254. 0.10
The default Subnet Mask is 255.255.0.0
Default login accounts:
- The meter has a set of default login credentials to access the front display, the webpages and ftp server.
The following login credentials are configured by default:
Table 1: For PM5000 firmware v2.9.9 and Earlier
For PM5000 model and firmware versions below:
B1. Webpages and FTP/FTPS
NOTE: More information on User Groups can be obtained from FA291653
Default IP address and login information unknown to login to the webpage and FTP server of PM5000 series meter
Product Line
PM5000 Series
Environment
Web server
Resolution
The default IP address is 169.254. 0.10
The default Subnet Mask is 255.255.0.0
Default login accounts:
- The meter has a set of default login credentials to access the front display, the webpages and ftp server.
The following login credentials are configured by default:
Table 1: For PM5000 firmware v2.9.9 and Earlier
For PM5000 model and firmware versions below:
- PM5560 / PM5562 / PM5563 / PM5580 meter models, and firmware v4.0.0 and above
- PM5570 / PM5660 / PM5760 meter models, and firmware v6.0.0 and above
- PM5650 meter model, and firmware v4.10.0 and above
- PM5561 meter model, and firmware v12.0.0 and above
- PM5661 / PM5761 meter models, and firmware v14.0.0 and above
- PM5570L / PM5660L / PM5760L meter models, and firmware v6.0.0 and above
- Username: it does not request a username
- Default password: 0000
B1. Webpages and FTP/FTPS
- Username: Administrator
- Default Password: MAC address which is unique for each Meter. Enter the MAC address of the meter without colon in capital letters (For example: if the MAC address of the meter is 00:80:f4:02:14:38, then password is 0080F4021438), which forced to change the default password for system security the first time you log in.
- Username: Guest
- Default Password: Powerlogic@1, but it's recommended to change the default password for system security the first time you log in.
NOTE: More information on User Groups can be obtained from FA291653
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: