Issue:
Current Product Design
Product Line:
Circuit Breaker Enclosures
Resolution:
No, the PowerPact P-Frame breakers with a motor operator CANNOT be installed in the current design P-Frame enclosures. The catalog numbers P1200S, P1200R, or P1200AWK.
NOTE: The motor operator MUST be factory installed in the breaker and it adds additional dimension to the front of the breaker that restrict the breaker from being installed in the enclosures.
Current Product Design
Product Line:
Circuit Breaker Enclosures
Resolution:
No, the PowerPact P-Frame breakers with a motor operator CANNOT be installed in the current design P-Frame enclosures. The catalog numbers P1200S, P1200R, or P1200AWK.
NOTE: The motor operator MUST be factory installed in the breaker and it adds additional dimension to the front of the breaker that restrict the breaker from being installed in the enclosures.