{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: PM8000 series meter default ICD files for IEC61850
Issue
A user needs PM8000 series meter default ICD files for IEC61850 communication configuration

Product Line
PM8000 Series meter

Environment
ICD files for IEC61850 communications

Resolution
The default ICD configuration files for IEC61850 communications are attached to this article

See Video below on how to create and load the CID file needed to enable IEC 61850 functionality

Schneider Electric Canada

Attachment(s)
PM8000_ICD_Files.zip [206.08 KB]