Search FAQs
What parts are replaceable on the XD4 and XD5 Joysticks?
Issue:
Replaceable XD4PA/XD5PA joystick
Product Line:
Push Buttons and Operator Interface
Environment:
22mm Joysticks
Resolution:
Check the system before ordering. Not all of these listed parts are loaded on the system.
The handle assemblies are as follows.
For the XD4 units:
ZD4PA12 2 direction, stay put
ZD4PA22 2 direction, spring return to zero position
ZD4PA14 4 direction, stay put
ZD4PA24 4 direction, spring return to zero position.
For the XD5 units:
ZD5PA12 2 direction, stay put
ZD5PA22 2 direction, spring return to zero position
ZD5PA14 4 direction, stay put
ZD5PA24 4 direction, spring return to zero position.
The contact block/body assemblies are as follows.
For the XD4 units:
ZD4PA103 for 2 direction controllers
ZD4PA203 for 4 direction controllers.
For the XD5 units:
ZD5PA103 for 2 direction controllers
ZD5PA203 for 4 direction controllers.
Replaceable XD4PA/XD5PA joystick
Product Line:
Push Buttons and Operator Interface
Environment:
22mm Joysticks
Resolution:
Check the system before ordering. Not all of these listed parts are loaded on the system.
The handle assemblies are as follows.
For the XD4 units:
ZD4PA12 2 direction, stay put
ZD4PA22 2 direction, spring return to zero position
ZD4PA14 4 direction, stay put
ZD4PA24 4 direction, spring return to zero position.
For the XD5 units:
ZD5PA12 2 direction, stay put
ZD5PA22 2 direction, spring return to zero position
ZD5PA14 4 direction, stay put
ZD5PA24 4 direction, spring return to zero position.
The contact block/body assemblies are as follows.
For the XD4 units:
ZD4PA103 for 2 direction controllers
ZD4PA203 for 4 direction controllers.
For the XD5 units:
ZD5PA103 for 2 direction controllers
ZD5PA203 for 4 direction controllers.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: