Search FAQs
Can the NSYTRAL210 terminals be cut?
Issue:
Modifying the NSYTRAL210 terminal block
Product Line:
NSY Terminal Blocks Jumpers, Linergy TR
Environment:
Terminal Blocks Jumpers, Linergy TR
Resolution:
Yes the NSYTRAL210 jumpers can be cut down. However this will cut the insulation. Suggest that there are 2, 3, 4, and 5 pole jumpers available and these should be used. See attached catalog page.
Modifying the NSYTRAL210 terminal block
Product Line:
NSY Terminal Blocks Jumpers, Linergy TR
Environment:
Terminal Blocks Jumpers, Linergy TR
Resolution:
Yes the NSYTRAL210 jumpers can be cut down. However this will cut the insulation. Suggest that there are 2, 3, 4, and 5 pole jumpers available and these should be used. See attached catalog page.
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: