{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for a QO130M200P, series S06 load center?
Issue:
Plug-On Neutral design repair parts

Product Line:
QO load centers

Resolution:
Only the parts listed below are considered field replaceable.
Cover - QOC30UF for flush or QOC30US for surface
Interior Assembly - QO130M200PI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K (contains parts to repair one hinge)
Door Latch Kit - 4020284450K
Main Circuit Breaker and Main Lug Keps Nut - 2342702001
NOTE:
The Load Center Directory label is part of the Cover, NOT the load center, BUT it cannot be purchased or sent out separately due to the UL Manifest on the label. It would require a brand new cover to be purchased. There is a Generic Directory label that only contains Lines and Numbers from 1 to 42 and the part number is LSDL.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: