Search FAQs
Are Solid Neutral Assemblies available(or can they be added) to ALL Double Throw Safety Switches, what neutral is used for each switch and what is the terminal lug data?
Issue:
Product FeaturesProduct Line:
Double Throw Safety Switch
Cause:
Terminal lug data
Resolution:
DTSS = Double Throw Safety Switch
S/N = Solid Neutral
Most of the DTSS will accept a S/N assembly with some exceptions. SEE the below S/N Table from the current on-line digest 178. Select the neutral based on the amperage of the switch.
** ALWAYS CHECK THE SWITCH WIRING DIAGRAM OR ON-LINE DIGEST FOR MOST UP TO DATE INFORMATION **
NOTES:
1) LOOK AT ALL APPROPRIATE FOOTNOTES UNDER THE TABLE
2) If a Catalog number contains a suffix 'N', then the switch will contain a S/N Assembly from the factory(for example: DTU224NRB or DTU324NRB).
3) For an existing(in the field), 400amp catalog number, it will require to check the switch wiring diagram and see if a field installable S/N assembly is shown. If a S/N is NOT shown on the wiring diagram, there will NOT be a field installable neutral.
4) All the 200amp Type DTU, Series E Switches come with a solid neutral factory installed.
5) The DT200N Neutral Assembly is provided with (4) lugs (2-incoming and 2-outgoing) with a wire range of (1) #4 AWG - 300kcmil AL/CU wires.
6) For Older Series Switches, SEE SWITCH WIRING DIAGRAM (located on the back side of the switch cover), IF THE SWITCH WILL ACCEPT A NEUTRAL ASSEMBLY.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: