{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the PM5500 series be revenue sealed?

Issue
How to revenue seal the PM5500 series meter from tampering.

Product Line
Powerlogic PM5500 series meter

Environment
Meter Hardware

Cause
Needs to revenue seal the PM5500 meter

Resolution
A sealing kit can be purchased for use with the PM5500 meter.  The kit comes with connector seals for the voltage and current inputs.  The connector seals cover protect the voltage and current inputs from physical tampering. The customer will need to provide their own security seals to be installed at the sealing points, point B on page 2 of installation guide below. (For example: Plastic Serialised Security Seal for meter terminal cover)

The part number for the kit is METSEPM55RSK.  Attached is the installation guide for the sealing kit.

Schneider Electric Canada

Attachment(s)
METSEPM55RSK.pdf [861.25 KB]