{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the Powerlogic Energy Meter be set to pulse out energy to an external device?
Issue
There is a need to communicate energy values from the meter to an external or monitoring program.

Product Line
Basic: EMB1010, EMB1021, EMB1032, EMB2010, EMB2021, EMB2032, EMB2043, EMB2083, EMB3010, EMB3021, EMB3032, EMB3043, EMB3083, EMB3084, and EMB3164

Extended Range: EME1010, EME1021, EME1032, EME2010, EME2021, EME2032, EME2043, EME2083, EME3010, EME3021, EME3032, EME3043, EME3083, EME3084, and EME3164

Environment
Existing installation that utilize the Powerlogic Energy Meters.

Cause
Need to communicate the energy from the meter to outside source.

Resolution
Using the Extended Range version of the meter (EMEXXXX), a pulse output can be set.
Pulse output: N.O., Opto-FET, 100 mA at 24 Vac/dc
Pulse rate: 0.10, 0.25, 0.50. or 1.00 kWh per pulse

Notes
  • The Basic version of the meter (EMBXXXX) cannot set a pulse output.
  • See attached document for the instruction bulletin and technical brochure

Schneider Electric Canada

Attachment(s)
POWERLOGIC_Energy_Meter_ Instruction_ Bulletin_63230-216-201A5.pdf [372.92 KB]
EnergyMeter_Technical_Data_3020HO0002R908.pdf [229.04 KB]