{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the G97 form code in a combination starter?
Issue:
Identifying the G97 form code in a combination starter.

Product Line:
8538, 8539, 8738, 8739 Combination Starters

Environment:
NEMA Contactors and Starters

Cause:
Product Selection and Specifications

Resolution:
G97 specifies an elapsed time meter which is externally mounted on the door or cover of a combination starter.  This option is not available with 24Vac control voltage.

Schneider Electric Canada