Search FAQs
Selecting Micrologic Device Type in Management Console
Issue
Incorrect selection of Micrologic device type can lead to lag communication and manual configuration of Vista default device diagrams.
Product Line
Software: ION Enterprise, Structureware Power Monitoring, Power Monitoring Expert
Circuit Breakers: Masterpact, Powerpact, Compact NS, Compact NSX
Environment
Applications with breaker communication with Schneider Electric power monitoring software
Cause
Need to select the correct device type for Micrologic circuit breaker
Resolution
The below tables display the correct device type for a given Micrologic trip unit type.
Incorrect selection of Micrologic device type can lead to lag communication and manual configuration of Vista default device diagrams.
Product Line
Software: ION Enterprise, Structureware Power Monitoring, Power Monitoring Expert
Circuit Breakers: Masterpact, Powerpact, Compact NS, Compact NSX
Environment
Applications with breaker communication with Schneider Electric power monitoring software
Cause
Need to select the correct device type for Micrologic circuit breaker
Resolution
The below tables display the correct device type for a given Micrologic trip unit type.
Trip Units | PME Device Type |
Micrologic 2.0 | No Communications |
Micrologic 3.0 | No Communications |
Micrologic 5.0 | No Communications |
Micrologic 2.0 Ammeter | Micrologic A or Micrologic A IFE_IFM |
Micrologic 3.0 Ammeter | Micrologic A or Micrologic A IFE_IFM |
Micrologic 5.0 Ammeter | Micrologic A or Micrologic A IFE_IFM |
Micrologic 6.0 Ammeter | Micrologic A or Micrologic A IFE_IFM |
Micrologic 7.0 Ammeter | Micrologic A or Micrologic A IFE_IFM |
Micrologic 2.0 Energy | Micrologic E or Micrologic E IFE_IFM |
Micrologic 3.0 Energy | Micrologic E or Micrologic E IFE_IFM |
Micrologic 5.0 Enegry | Micrologic E or Micrologic E IFE_IFM |
Micrologic 6.0 Energy | Micrologic E or Micrologic E IFE_IFM |
Micrologic 5.0 Power | Micrologic P or Micrologic P IFE_IFM |
Micrologic 6.0 Power | Micrologic P or Micrologic P IFE_IFM |
Micrologic 7.0 Power | Micrologic P or Micrologic P IFE_IFM |
Micrologic 5.0 Harmonic | Micrologic H or Micrologic H IFE_IFM |
Micrologic 6.0 Harmonic | Micrologic H or Micrologic H IFE_IFM |
Micrologic 7.0 Harmonic | Micrologic H or Micrologic H IFE_IFM |
Trip Units | PME Device Type |
Micrologic 2.2 | No Communications |
Micrologic 2.3 | No Communications |
Micrologic 3.2 | No Communications |
Micrologic 3.3 | No Communications |
Micrologic 5.2 Ammeter | Micrologic A Compact NSX |
Micrologic 6.2 Ammeter | Micrologic A Compact NSX |
Micrologic 5.3 Ammeter | Micrologic A Compact NSX |
Micrologic 6.3 Ammeter | Micrologic A Compact NSX |
Micrologic 5.2 Energy | Micrologic E Compact NSX |
Micrologic 6.2 Energy | Micrologic E Compact NSX |
Micrologic 5.3 Energy | Micrologic E Compact NSX |
Micrologic 6.3 Energy | Micrologic E Compact NSX |
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: